Custom Motion Commands
Call Flowchart:

Example of implementing a custom Motion Command: Step 1: Set motion parameters Step 2: Call SendCmd to send to Controller.
Implement Command PMoveL(point, speed, zone, tool, wobj); This command is similar to the current MOVEL Command. Users can implement their own logic inside the command, such as pairing with a welding machine.
/**
* @brief Implement Command PMoveL
*/
void RegPMoveL() {
// 1. Command configuration, such as name, trigger method, task limits, etc.
RLCmdConfigAPI cfg;
cfg.SetFuncName("pmovel");
// Set command look-ahead method to Motion Command
cfg.SetLookAhead(CmdLookAheadImplAPI::MOVEMENT_ITSELF) ;
// Set task limit type
cfg.SetTaskLimit(TaskLimitAPI::TASK_NO_LIMIT);
// Set step-back type
cfg.SetStepBack(StepBackAPI::STEP_BACK_CUSTOM);
// 2. Create command according to configuration
BEGIN_COMMAND_API(cfg)
// 3. Configure parameter checker for the command
PARAMS_API(
ArgTypeAPI(ValueTypeAPI::VALUE_ROBTARGET),
ArgTypeAPI(ValueTypeAPI::VALUE_SPEED),
ArgTypeAPI(ValueTypeAPI::VALUE_ZONE),
ArgTypeAPI(ValueTypeAPI::VALUE_TOOL),
ArgTypeAPI(ValueTypeAPI::VALUE_WOBJ)
)
// 4. Command forward execution body
RLCmdActionAPI cmd_func = [=](std::shared_ptr<RLCallFrameAPI> frame,
std::vector<std::shared_ptr<SymbolVarBaseAPI>> args) -> CommandExecuteAPI {
// Get parameter data
auto point = args[0]->GetPointAPI();
auto speed = args[1]->GetSpeedAPI();
auto zone = args[2]->GetZoneAPI();
auto tool = args[3]->GetToolAPI();
auto wobj = args[4]->GetWobjAPI();
CommandExecuteAPI cmd_exec = [=]()
{
MotionCmdArgsAPI args_api;
// Set target point
args_api.SetTargetPoint(point);
// Set motion type to linear
args_api.SetMoveType(MoveTypeAPI::MOVE_L);
// Set tool speed zone information
args_api.SetTool(tool);
args_api.SetWobj(wobj);
args_api.SetZone(zone);
args_api.SetSpeed(speed);
// Set pointer to current execution position
args_api.SetUpdatePointer(frame->GetCmdTask(), frame->GetCmdFile(), frame->GetCmdLine());
// Set trigger
TriggerAPI t;
t.type = TriggerAPI::TriggerType::DISTANCE;
t.reference_is_from_start = true;
t.value_from_reference = 0.1;
t.trigger_callback = [=]
{
LOG_DEBUG<<frame->GetCmdTask()<<" "<<frame->GetCmdFile()<<" "<<frame->GetCmdLine()<<" 100mm trigger callback";
};
args_api.SetTriggers({t});
// Set path callbacks
args_api.SetCallback(CallBackTypeAPI::MOVE_START,[]{LOG_INFO<<"movel start callback";});
args_api.SetCallback(CallBackTypeAPI::MOVE_FINISH,[]{LOG_INFO<<"movel finish callback";});
args_api.SetCallback(CallBackTypeAPI::MOVE_PAUSE,[]{LOG_INFO<<"movel pause callback";});
MotionCmdAPI api;
// Send command
int ret = api.SendCmd(args_api);
LOG_INFO<<"send motion cmd:"<<ret;
LOG_DEBUG<<"point:"<<point<<" speed:"<<speed<<" zone:"<<zone
<<" tool:"<<tool<<" wobj:"<<wobj;
LOG_DEBUG<<":"<<frame->GetCmdTask()<<" "<<frame->GetCmdFile()<<" "<<frame->GetCmdLine();
if (ret == 0){
return CommandProcessResultAPI::CMD_PROCESS_EXTRA;
}else{
return CommandProcessResultAPI::CMD_PROCESS_ERROR;
}
};
return cmd_exec;
};
EXECUTE_API(cmd_func)
// 5. Register command to Controller
REGISTER_COMMAND_API
}
After the above steps, a new Motion Command is created. The PMoveL command can now be called in RL. For more command usage, please refer to examples/motion_cmd.cpp